AnsweredAssumed Answered

BSP_ALARM_FREQUENCY in TWRK60N512 set to 100 ??

Question asked by Luca Gotti on Jun 3, 2011
Latest reply on Jun 13, 2011 by Petr Uhlir

In all the MQX documentation ( and on this forum too .. )  it's clearly stated that the minimun tick delay of MQX is 5 ms which means that the macro BSP_ALARM_FREQUENCY is set to 200 ( 1000 / 200 = 5 ms ) .

Today I've cheched the BSP_ALARM_FREQUENCY value for TWRK60 BSP and i found it's 100 ( which means 10 ms minumum delay  time )... 

I'd like to know what is the reason of this settings and , more important, if there is any problem to set this value to a greater value ( like 500   ).

 

 

Outcomes