Is there a complete example of a simple TCP sockets client around somewhere? Found a server (quote-a-day?), but no client.
I have an app that works fine under Linux on an Intel box, but after some modifications for MQX and a lot of head banging, I still don't have something that connects and talks to the server. I was getting it to connect to the server, but adding in the recv call was crashing the code completely (as in, before it even got to the recv call). Then I figured out that the task needed more stack space, increased it to 4000 or 6000 and it no longer crashes, but it also no longer connects.
FWIW, I'm running on a very old M52233DEMO board, so I'm thinking I may also need to patch the phy_mfc5223x.c code for the speed problem?
John
From Technical Support I got a server-client example but it is for the MCF52259.
You can easily port it to your system.