We have two floating standard licenses.
I have installed RedHat Linux 8 in a virtual machine, whose MAC has been used to register the products.
Once I have set the lmgrd service on, we have tried to use it with the following results: at first, verything went OK, but later compilation and loading is going at a very low speed.
From the lmgrd log, we can see all features seem to be detected OK:
Dbug output from metrowks seems a little more scary, see a sample:
For every client, we get the following set of lines:
What is happening? There seems to be lots of problemas, but the install has been fresh, and using the recommended practices.
TIA, and best regards.
More data: When I try to compile C++ sources, it will only report not finding ProfessionalEditionMCU and fail compilation.
It seems in the case of the C compiler, it is looking for the first edition that gives the license, and it finds that onñly Special edition will fail.
But, of course that should be so: There is no feature '****EditionMCU" in the lcense.dat file!
There are features sucha as Win32_CWIDE_Unlimited for instance.
May there be an error in the license management system???
If you are having network latency issues, you probably should not be using a floating license.
Second, make sure that your IT department has opened the IP ports that FlexLM uses to communicate. They will insist that they have done this, but in a number of the floating license problems I have dealt with, after several weeks of trials it comes down to the fact that they did not open the ports.
Finally, if you have not done so already, file an on-line service request on this.
---Tom
No, I have no latency issues (ping response time ~ 0.4 ms)
I *am* the IT department; i know all ports are open.
Of course; I will file a request. I just hoped someone had already lived vthrough this, and there was a quick answer.
Thanks!