I understand that the 'newer' 56k parts do not support direct control via the SCI port as the older 56k parts did. I would like to control the 56371 via simple ascii commands from a RS232 port.
Are there any application notes describing a minimal control via a serial connection?
I'm considering using a 68xx (or a PIC) such that the (micro)USART would connect to the PC com port and the SPI port (of the micro) would connect to the 56371.
Any simpler ideas or suggestions?
Thanks,
TomC
Hi Tom,
it seems that noone replied to your post since there is not better idea to esablish an asynchronous serial interface communication with the DSP than using a microcontroller. Just take that one you likle best and use an according application note for realization.Most MCU vendors support those bread and butter interfaces by code examples.
Good luck - Christian