AnsweredAssumed Answered

Simple RTC causing unhandled interrupt

Question asked by Marco Fratini on Apr 15, 2011
Latest reply on Apr 22, 2011 by Marco Fratini

Hi everyody. I'm using MCF52259demokit and MQX 3.6. I'm fightint against the main task that after 2 or 3 hours of running (or debugging) launches an unhandled interrupt. The only peripheral I'm using is the RTC with 1Hz interrupt. So I think that RTC must be the cause of the issue.

 

I'm attaching the code for anyone who wants to try it, or take a look at it to see if there is something wrong. 

 

Regards,

Marco

Outcomes