hello,
i want to start learning progamming. i have some board with the power pc mpc5200b with external flash memory.
i have one code warrior usb tap. but i dont have the software and usb drivers to progamming the mpc5200b core.
wich software do i need?
best regards
Solved! Go to Solution.
You will want to download CodeWarror for mobileGT, which supports the processor type. Information about these tools and a download link can be found on this web page.
---Tom
You will want to download CodeWarror for mobileGT, which supports the processor type. Information about these tools and a download link can be found on this web page.
---Tom
hello,
thanx tom for the download link! after i downlaod the the software i cant connect to my core.
target core:mpc5200b habanero connect to code warrior usb tap.
i download the datsheet from the mpc5200b. and use the follow pins: use 16 pin j-tag cop connector)
BO4 j-tag tck
A02 j-tag tdo
AO3 j-tag tdi
A04 j-tag tms
A14 sreset
B13 hreset
my target dont support B03 j-tag trst. and i dont have CKSO,QACK on the board
when i go to:hardware diagnostic and i try to connect to the core( test begin scoop loop) i dont see the run/pause led working. all the time the rx/tx led is working and stay green.
i hope i provide all the information to get some help.
bet regards.