Israel Grimaldo

Communication problem with  DEMO09S08QG8 board

Discussion created by Israel Grimaldo on Mar 10, 2011
Latest reply on Mar 10, 2011 by David Payne

I got a DEMO09S08QG8 board and I already programmed a M9S08QG8 chip using the integrated USB-to-BDM interface of the board in an external target. Now I want to do the same with a MC9S08SE8CRL chip but there is no communiation with the target when I run the debug mode in CodeWarrior V6.3.

 

My question is, what I need to change in the board configuration? Could it be the 3.3V power of the BDM Port and change it for an external 5v power?? 

 

Thak you.

Outcomes