Hello All,
The latest OSBDM build version 29.04 has been released by P&E Microcomputer Systems. It includes Firmware/Drivers source files, circuit diagrams, BOMs, virtual serial port and firmware update utilities as well as a design guide. The latest OSBDM firmware and drivers support new features such as automatic firmware update (under Codewarrior 10.1 and newer), virtual serial port and trim for HCS08/RS08/CFV1 devices.
OSBDM build version 29.04 includes embedded support for HCS08, RS08, Coldfire V1, Coldfire V234, Kinetis ARM, HC(S)12(X), DSC, and Qorivva MPC55xx/56xx Freescale architectures.
To download the latest OSBDM design package and learn more about this embedded hardware interface, please go to:
Best Regards
Zahar
P&E Microcomputer Systems.
Dear Zahar,
I wonder if you can solve my question in this post :
https://community.freescale.com/message/93606#93606
I want to know if Codewarrior 7.1 and 7.2 support OSBDM version 26, which is being required in order to work in CW 10, but I wouldn't want to lose contact in CW 7.1.
Your help will be really appreciated,
Many thanks and regards,