HI-WAVE Warning: "DBG module is armed. Disarm?"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HI-WAVE Warning: "DBG module is armed. Disarm?"

Jump to solution
857 Views
carloscuev
Contributor V

Im working with a Witztronics hardware with updated USBDM v4.4-Beta Firmware. Im programming a S08JM60, Every breakpoint or debug command (except Start, Single Step and Step Over), hiwave keeps asking me  "DBG module is armed. Disarm?" and clicking "Yes" or "No" it works fine, I can debug without any problem, but the popup window is quite annoying, Is there something cand be done about this?

Tags (2)
0 Kudos
1 Solution
309 Views
carloscuev
Contributor V

Solution Found:

In Debugger Check Option "HCS08 Open Source BDM->Trigger Module Settings->General Settings->Disarm automatically the module when debugger stops"

 

Now I like more USBDM than USB-MULTILINK-BDM :smileyvery-happy:

View solution in original post

0 Kudos
1 Reply
310 Views
carloscuev
Contributor V

Solution Found:

In Debugger Check Option "HCS08 Open Source BDM->Trigger Module Settings->General Settings->Disarm automatically the module when debugger stops"

 

Now I like more USBDM than USB-MULTILINK-BDM :smileyvery-happy:

0 Kudos