Joe Kissell

Combine App & Bootloader - CW6.3, Coldfire V1, MCF51CN128

Discussion created by Joe Kissell on Jan 31, 2011
Latest reply on Jun 12, 2013 by ZhangJennie

I've seen lots of referrences to using an HEXFILE command in the PRM file for the purpose of adding your Bootloader's S19 file into your Application code. The output S19 can then be given to production so they only have to flash one file.

 

However, this doesn't seem to work with my project. I have a LCF file instead of a PRM file and it doesn't seem to allow me to add commands like HEXFILE.

 

Can someone please help?

Outcomes