When rebuilding MQX Libraries as per “FSL_MQX_Getting_Started.pdf”, section 2.4 (Freescale CodeWarrior Development Studio Version 10), when switching between targets (Debug to Release), there are several warnings concerning “Invalid project path: Duplicate path entries.” See attached image.
The build process seems to work. Should I be concerned about these warnings? How do I fix them?
Thanks,
Juan
Codewarrior 10 Special Edition
Windows XP Pro
MQX 3.6.2
PEMicro USB ColdFire Multilink.
Custom Target based on Coldfire MCF52259.
Solved! Go to Solution.
Hi Juan,
I think I found the issue. I didn't have that warning with the "Release" target but had one wanring with the "Debug" target.
I tracked it down to having duplicate include paths. Look at the attacked file.
Once I deleted the bonus path (the highlighted path on picture) the warning went away after re-compile.
Hope this solves your problem.
Regards,
David
Hi Juan,
I think I found the issue. I didn't have that warning with the "Release" target but had one wanring with the "Debug" target.
I tracked it down to having duplicate include paths. Look at the attacked file.
Once I deleted the bonus path (the highlighted path on picture) the warning went away after re-compile.
Hope this solves your problem.
Regards,
David
Hello David,
I see. Just was curious if it was a major issue since my mqx libraries seem to compile correctly. I will try it out when I get back to the office.
Thanks,
Juan