Hello,
It is my first time to write an application with a main program in a file and several subroutines in different files for a HCS08QE MCU. Attached is a program for testing. After compling it, I got the following message:
A13003: Value is truncated to one byte
SR_Test.asm line 3
A13003: Value is truncated to one byte
SR_Test.asm line 4
A1104: Undeclared user defined symbol: PTCD
SR_Test.asm line 3
Compile failed
The compiler regards the command "BSET 7,PTCD" in the main program as a direct addressing instruction since the address of PTCD is 0x04. However, it is not the case for the same command in the subroutine.
I tried many times by adding XDEF, XREF, XREF.B to the .asm files, and the object code file to Project.prm, but I got other error messages.
Please give me advice because I have spend a long time to learn this which should be a straightforward issue.
Thanks.
Solved! Go to Solution.
Hello
I assume you want to build the 2 .asm file separately and then link them together.
Am I right?
Then you should
1- Create a file SR_Test.inc, where you have declaration for all symbols from SR_Test.asm
that are visible from outside of the file.
2- Include that .inc file in main.asm and remove include from SR_Test.asm
3. In SR_Test.asm, include directive.inc and make label SR_Test_Function visible from
outside of the module (using directive XDEF)
CrasyCat
Hello
I assume you want to build the 2 .asm file separately and then link them together.
Am I right?
Then you should
1- Create a file SR_Test.inc, where you have declaration for all symbols from SR_Test.asm
that are visible from outside of the file.
2- Include that .inc file in main.asm and remove include from SR_Test.asm
3. In SR_Test.asm, include directive.inc and make label SR_Test_Function visible from
outside of the module (using directive XDEF)
CrasyCat
Thank you, CrasyCat,
It works. This is what I need.
sctang