CodeWarrior V10 V7.2 and V6.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior V10 V7.2 and V6.2

596 Views
TeeTwo
Contributor I

I would like to use one IDE across three different ColdFire CPU MCF51CN, MCF5225, and MCF5441x. I can install and get V6.2 to work with the 51CN examples. I am having no luck using V10 to work with the 51CN. Is it possible to use CW V10 to work across all of these platform? If so what are some of the common mistakes folks make when trying to use V10 with a 51CN?

 

Thanks in advance for your reply

Labels (1)
0 Kudos
1 Reply

171 Views
CrasyCat
Specialist III

Hello

 

CodeWarrior MCU V10 should support all Coldfire MCUs.

 

Which kind of trouble are you facing?

Are you unable to build, to debug, ...?

 

Did you try creating a new project for MCF51CN128. Can you build and debug it?

 

CrasyCat

 

0 Kudos