The Processor Expert will not generate code after a new component has been added. The status area always shows "66%", but afterwards no additional code was added nor any cpu.c modifications made. It had been working fine for weeks, then mysteriously stopped.
Hi,
I have the same probleme with CW10.1 and device initialization no code is genarate. Also no MCUInit the compilation failed.
Hello,
Nobody for answer ? CW10.1 go to the garbage, i work with CW 10.0...
Domi
Hello
I did create a project for HCS08AC8, where I did enable Device Initialization.
I am able to generate code and add devices to configure there.
So this seems to be working just fine.
I would recommend you to submit a service request for that.
Click here to submit a service request.
Make sure to attach a reproducible project and installed product information to the service request.
CrasyCat
Hello,
It's ok in win 7 pro64 with "run as administrator"
Domi