I'm am using a MC9S08JM16 chip with a IR receiver attached to the IRQ line (external interrupt). Now I'm using the CodeWarrior for microcontrollers v10.0. I'm also using the Processor Expert to create modules such as UART. However, there is no useful IR module. I've also tried searching for "IR", "infrared", "decoder" and other combos in the support sections and have not come up with anything useful. Basically, what I'm curious to know is if there is any sample code, helpful hints, or something that explains how to set up an IR decoding protocol with the IDE and chip I'm using, anyone have any ideas?
Hello,
could you please specify what kind of protocol the transmitter use? Do you need to decode RC-5 protocol?
best regards
Vojtech Filip
Processor Expert Support Team
/Unfortunately, I don't know what protocol the IR transmitter remote uses. I do know that it is a Remotec BW7070 universal remote, but that is it. The IR receiver I'm using is an Osram SFH5110. When attaching an oscilloscope to the data line of the receiver, I can determine the binary, and therefore the hex value of each signal the receiver sends to the JM16. I could give a list of the hex values if that would help. I also know the bit length of the start, one, and zero bits as well as the period. Will that make things easier?
Start bit = 19ms
One bit = 38ms
Zero bit = 67ms
Period = 115ms
data signals:
0x30
0x3F
0x37
0x28
0x17
0x0F
0x2F
0x1F