AnsweredAssumed Answered

Connection problem with CW10.0

Question asked by Gabriel Soccodato on Dec 3, 2010
Latest reply on Jan 29, 2011 by Gabriel Soccodato

Hi,

 

I have made a hardware implementing jm60OSBDM for HCS08 and CFV1.

With HCS08 It works for CW6.3 but It doesn't work with CW10.0.

I can't download the code to the MCU.

If I set a project to work with both P&E BDM and OSBDM, and at first I use P&E BDM and then OSBDM it works.

But with OSBDM only I can't make it work. I've tried with different firmware and drivers versions.

Has someone had a similar problem?

 

Best regards,

 

Gabriel

Outcomes