Masmiseim

M52233Demo Board with Codewarrior v10

Discussion created by Masmiseim on Dec 2, 2010
Latest reply on Dec 2, 2010 by Masmiseim

Hello,

 

I Try to use the M52233Demo Board with Codewarrior v10, using the BDM on the Evalboard.

Windows recognize the Board as “Jungo USB Multilink 2.0” in the Device Manager.

I ‘m not able to get a connection to the BDM in Codewarrior.

I’ve tried OSBDM ==> Error: “Coldfire GDI Protocol Adapter: Can’t connect. The Debugger can not load the OSBDM DLL!

And PnE BDM ==> Error: “Coldfire GDI Protocal Adapter: Can’t connect. The Debugger can not connect to the PE BDC interface or targeted hardware board.

 

Any suggestion?

 

Greetings

Outcomes