AnsweredAssumed Answered

TWR-K40X256 - serial transmission on MQX 3.6.2 beta (for k40) doesn´t works

Question asked by Paz Rodolfo on Nov 25, 2010
Latest reply on Jan 5, 2011 by Denys Yurchenko

 

I was testing the new MQX for the k40 but the serial transmission doesn´t works, I also rebuild
the bsp_twrk40x256 project with this options in the user_config.h:

 

#define BSPCFG_ENABLE_TTYA       1//

 

#define BSPCFG_ENABLE_ITTYA      0

 

#define BSPCFG_ENABLE_TTYB       1

 

#define BSPCFG_ENABLE_ITTYB      0
#define BSPCFG_ENABLE_TTYC       1
#define BSPCFG_ENABLE_ITTYC      0
#define BSPCFG_ENABLE_TTYD       1//
#define BSPCFG_ENABLE_ITTYD      0
#define BSPCFG_ENABLE_TTYE       1
#define BSPCFG_ENABLE_ITTYE      0
#define BSPCFG_ENABLE_TTYF       1
#define BSPCFG_ENABLE_ITTYF      0
#define BSPCFG_ENABLE_I2C0       0
#define BSPCFG_ENABLE_II2C0      0
#define BSPCFG_ENABLE_I2C1       1
#define BSPCFG_ENABLE_II2C1      1
#define BSPCFG_ENABLE_SPI0       0
#define BSPCFG_ENABLE_ISPI0      0
#define BSPCFG_ENABLE_SPI1       0
#define BSPCFG_ENABLE_ISPI1      0
#define BSPCFG_ENABLE_SPI2       0
#define BSPCFG_ENABLE_ISPI2      0
#define BSPCFG_ENABLE_GPIODEV    1
#define BSPCFG_ENABLE_RTCDEV     1
#define BSPCFG_ENABLE_PCFLASH    0
#define BSPCFG_ENABLE_ADC0       0
#define BSPCFG_ENABLE_ADC1       1
#define BSPCFG_ENABLE_FLASHX     0
#define BSPCFG_ENABLE_ESDHC      0
The project that I was testing is the adc example, when the project 
is compiled and debugged doesn´t appear mistakes but when you try to send a data 
by the serial port using "printf" the data is never sended.  
I hope some one can help me to solve this.
Best regards.

 

 

 

 

 

 

 

Outcomes