Jorgen Sandberg

Code Warrior 10 - failed connection to P&E USB Multilink Interface rev C

Discussion created by Jorgen Sandberg on Nov 12, 2010
Latest reply on Jan 4, 2011 by DAVE BARTLETT

I have installed the Code Warrior 10 on Windows 7 (32 bit). I have attached the P&E USB Multilink Interface Rev C to my PC and to the taget (an MC9S08SV16).

 

I have a program in C that compiles and builds without errors.

 

When I try to program the flash I get the message:

 

Beginning Operation...

____________________

Initializing remote connection...

Performing target initialization...

Error:   Connect Failed.

Can't connect. The Debugger can not connect to the P&E device (HC GDI Protocol Adapter)

Error:  command failed

 

Please, if anyone knows the remedy, please inform me.

 

The P&E USB Multilink Interface is about 2 years old.

 

Regards,

Jorgen

Outcomes