Hello~~
I installed Beekit 1.9.17 onto a Windows 7.
When I launch Test tool from Beekit. The communication settings found no comport of my device (see attached picture). However, my device is shown in the Device manager window. My device is a SBR board with CP2102 as the virtual comport interface.
I can use the same board to communicate with Hyperterminal or other serial program.
I wonder whether this is because of the CP2102's driver version. I am using the Silab driver included with Beekit.
But Test tool failed to found my device as described above.
When I use the same board on another PC (with older version of CP2102). Everything work fine.
Please help....
Many thanks.
I have the same problem.
Try to run the Test Tool as Administrator and It will works with others virtual COM.