Integrating FNET with MQX on the Tower 52259

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Integrating FNET with MQX on the Tower 52259

Jump to solution
914 Views
accutime
Contributor III

Hi

 

Has anybody actually got FNET functioning with MQX ?

 

Is so would they supply infomation on the mapping file  "intflash.lcf" and a simple step by step guide of the integration

 

I am using the 52259 Tower Development System but it should be very similar for other V2 platforms

 

Thanks in Advance

 

Paul H

 

0 Kudos
1 Solution
354 Views
butok
NXP Employee
NXP Employee

Hi Paul,

 

You can look at this "unofficial" AN:

http://netcologne.dl.sourceforge.net/project/fnet/fnet/AN/FNET_and_MQX%20Rev%201.3.pdf

 

Best regards,

Andrey Butok

 

View solution in original post

0 Kudos
2 Replies
354 Views
accutime
Contributor III

Hi

 

Thanks for the document. (probably needs checking over for a few typos)

 

FNET working perfectly .

 

HIGHLY RECOMMENDED

 

Thanks

 

 

0 Kudos
355 Views
butok
NXP Employee
NXP Employee

Hi Paul,

 

You can look at this "unofficial" AN:

http://netcologne.dl.sourceforge.net/project/fnet/fnet/AN/FNET_and_MQX%20Rev%201.3.pdf

 

Best regards,

Andrey Butok

 

0 Kudos