CW10.0 nogo with DEMOJM board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW10.0 nogo with DEMOJM board

740 Views
donw
Contributor IV

Hi all

I am trying to get CW v10 to download code to the P&E DemoJM board, which has the P&E multilink built-in.

(Win7, 64 bit machine)

The board works OK under CW 6.1. (XP system)

The 'P&E Connection Assistant' in the debugger shows that the board is connected 'USB-ML12: DEMOJM on USB1'

but it just says 'an error occurred, retry'  when trying to download code.

and gives the error message 'HC GDI Protocol Adapter:  Can't connect . The debugger cannot connect to the PE device.' when quitting the connection.

The first time I connected there was a (fast) code update of the multilink code in the board.

 

the HCS08 debugger is 10.0.0.FSL_b2619

 

Has anyone had CW working with this board? (or is there a bug as in CW v6.3+ which has the same problem)

Labels (1)
0 Kudos
1 Reply

203 Views
sebasira
Senior Contributor I

Hi!

 

I'm having the same problem... Have you solved it? Has anyone get it to work?

 

Demo JM doesn't work with CW 10 not on a win 7 x64, not even on win XP x32

0 Kudos