I am a Ubuntu Lucid Linux User! I installed the CodeWarrior Development Studio v10. The installation was OK. However, I am getting an error when I run cwide (see below). The problem seems to be in the library libpemicro_jloaderh.so.
Can someone help me?
Looking at the CodeWarrior V10 product page, I only see RedHat Linux mentioned as the supported Linux implementation.
---Tom
Yes, you are right! But... In the CodeWarrior README.txt file, there are instructions to install it in several others linux flavors. (See below!) I followed the instructions for Ubuntu 9.10. But ... It did not work! :smileysad:
=========================================
=========================================
I stand corrected. You will probably have to file a service request n this, but before you do, check the following:
1) That you are using are using 32-bit Ubuntu.
2) The error messages are coming from the JRE, so verify that the Java version you are using matches the requirements.
---Tom