Jeff Brown

CW10, Flash programmer.

Discussion created by Jeff Brown on Jul 25, 2010
Latest reply on Jan 19, 2011 by Greg Topel

Is anyone getting any use out of CW10?

 

I am using an MCF52259 processor  with the PE Multilink, and running CW10 on an XP machine.

This project was imported to CW10 from CW7.1.2.

 

I am choosing the Flash File to Device from the Flash Programmer Icon.  I chose the elf file to program and here are the results as seen in the console window:

 

 

fl::target -lc "CW10 Debug Bootloader - CW10 Debug Bootloader - PEMICRO_USB"

fl::target -b 0x20000000 0xffff

fl::target -v off -l off -ie on -i "C:/Projects/CW10/USB-DebugBootloader/CW10 Debug Bootloader/../cfg/mcf52259_internal_flash.cfg" -p 52259

 

Error: no such processor "52259"

 

How can it not find the processor?

the *.cfg file that it is using is from the debugger section from the original project.

 

Anyone have any ideas of what i need to do?

Outcomes