Hi,
I am unable to add a New Source Folder to my project, a regular folder, no problem. I either get an error stating the Root name must be entered or Invalid Project path: Duplicate path entries, even when I browse. It does not matter what I type as the folder name. Also, could you point me to the documentation that describes the features and/or privileges that a source folder has over a regular folder as it related to the project.
Thanks,
Will
Solved! Go to Solution.
Hi,
Update, the inability to add a New Source Folder problem was as the error indicated a "duplicate path exists". However, the problem is that the project built successfully (no errors) and the duplicate path existed in the setup for Path and Symbols/Includes. I do not know how the duplicate entry was creatded. In this case the error can be duplicated by explicitly specifying a path such as c:/CW10/workspace/myProject/Sources and ${ProjDirPath}/Sources. It does not matter if the duplicates are in the same languages folder or not, in my case they were not.
Regards,
Will
Hi,
Update, the inability to add a New Source Folder problem was as the error indicated a "duplicate path exists". However, the problem is that the project built successfully (no errors) and the duplicate path existed in the setup for Path and Symbols/Includes. I do not know how the duplicate entry was creatded. In this case the error can be duplicated by explicitly specifying a path such as c:/CW10/workspace/myProject/Sources and ${ProjDirPath}/Sources. It does not matter if the duplicates are in the same languages folder or not, in my case they were not.
Regards,
Will
Please file a service request so this problem can be looked into. Click here to do that.