Error in MCF52223RM ?!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in MCF52223RM ?!

558 Views
AnteOO
Contributor II

 

Hi! On page 25-25 in the MCF52223RM, it says
"

 

The ADC consists of a cyclic, algorithmic architecture using two recursive sub-ranging sections (RSD#1

and RSD#2), shown in

clock, resulting in an overall conversion rate of two bits per clock cycle. Each sub-ranging section is

designed to run at a maximum clock speed of 5.0 MHz. Thus a complete 12-bit conversion takes 6 ADC

clocks (1.2ms), not including sample or post processing time."

 

 

I'm guessing that it should be µs, instead of ms :smileywink:

 

just in case you want to change it!

I found no other way of contacting freescale, save starting a support errand...

Labels (1)
0 Kudos
1 Reply

271 Views
scifi
Senior Contributor I

Hi!

 

You are not the first one to notice this:

 

https://community.freescale.com/message/62324#62324

 

Thanks for sharing, anyway.

0 Kudos