Hi,
in my product I'm utilizing MQX 3.5.1 with USB Host + MFS. My uart0 is used as bus 485 and the port 2 of UA register is setted as output but when there is the usb init this port is setted from MQX as input ... there is a reason? Can I try again to set this port as output or I cause the bad functioning of USB stack?
Thanks,
what board do you use?
m52259demo board
USB_VBUSD is muxed with RTS0 (detects whether VBUS is on or off when configured as a device).
Thanks for the reply,
so if I understand well when I try to set this port as output I don't cause the bad functioning of USB stack because I'm using only the USB Host mode.
Yes, you can set it as output if you are concerned only to USB device. Note, that there is still CTS0, that can be driven by UART or by USB module. In the host mode, this must be driven by USB, so it is not possible to drive CTS0 when USB is in host mode.