Yesterday, the code warrior of IDE version 5.9.0 was re-installed after several tries of debugging the core 0 of P2020.
Then, I downloaded the service pack 8.8.3 so that there is support for QorIQ processor.
After installing the code warrior, I unzipped the PA_8.8.x_P2020_ServicePack_0850.zip to the
C:\Program Files\Freescale\CodeWarrior PA V8.8 which has support of USB-TAP for P2020 processors.
with P2020RDB connected to the USB-TAP,
I pressed debug(F5) on the IDE. I encountered the error given in the screen capture.
I tried a few times but still fail to access the P2020 core 0 and core 1 with the Code Warrior IDE.
Please give me some direction of how I should approach the problem.
Solved! Go to Solution.
Based on the advice from online Freescale TechnicaI Support,
I no longer see the problem of CCSProtocolPlugin:Error writing memory [SAP: write over-flow] after installing the service pack 1 from CodeWarrior Development Tools->CodeWarrior Downloads->Updates and Patches->CodeWarrior for Power Architecture Technology Updates for CodeWarrior for Power Architectures (Netcomm) v8.7-8.8->CodeWarrior Power Architecture 8.8 Service Pack 1 for P2020, 8572, 8315 & 8569.
The zip file PA_8.8.x_P2020_ServicePack_0850.zip I talked about in my previous post was found in p2020 3rd linux DVD.
Just in case some users may not be able to read attachement.
I shall write down the error message given by the debugger
CCSProtocolPlugin:Error writing memory
[SAP: write over-flow]
Has anybody encountered this error before?
Need help and advice here.
Based on the advice from online Freescale TechnicaI Support,
I no longer see the problem of CCSProtocolPlugin:Error writing memory [SAP: write over-flow] after installing the service pack 1 from CodeWarrior Development Tools->CodeWarrior Downloads->Updates and Patches->CodeWarrior for Power Architecture Technology Updates for CodeWarrior for Power Architectures (Netcomm) v8.7-8.8->CodeWarrior Power Architecture 8.8 Service Pack 1 for P2020, 8572, 8315 & 8569.