Hi,
CW 7.1.2, MQX 3.4, M52259EVB
My USB host application is working fine in Debug Mode but there is a problem in Int Flash Release mode.
Every time when I insert the USB stick I got this error:
************************************************************************
Vendor Information: Mass Storage Device
Product Identification: Flash Disk
Product Revision Level: 8.07
************************************************************************
Error while opening partition (UNKNOWN ERROR !!!)
Device removed, starting device cleanup
--->Closing MFS
--->Uninstalling
--->Uninstalling PM
--->Closing disk
After that I have to restart microcontroller to use USB again.
I've check my application, web_hvac and mfs_usb examples with freescale and kingston sticks so far.
Any ideas?
Regards,
tomaszk
Hello,
this is known bug of CodeWarrior compiler. I recommend to use CW7.2.