Hi,
I am trying to boot the ads5121 board using NFS. I restarted the NFS server and teh output is shown in the attached txt file nfs server.txt.
I also printed the env in u-boot and the output is found in the attached file u-boot.txt.
When I tried to boot the board with the nfs option I ot an error. The output is shown in the attached file nfsrun.txt.
My host machine is running under Centos 4.7 and my target is the ads512101 board rev 3.0. I installed the BSP from the LTIB iso file found on freescale.com (MPC512xADS_20090603-ltib.iso). I am guessing that maybe the ltib file is the worng one.
Can someone please help me?
Thank you in advance.
Solved! Go to Solution.
Hi¡
Have you followed steps of MPC5121 Porting Linux app note ?
http://www.freescale.com/files/32bit/doc/app_note/AN3765.pdf
Is very good explained, tell me about problems.
Hi¡
Have you followed steps of MPC5121 Porting Linux app note ?
http://www.freescale.com/files/32bit/doc/app_note/AN3765.pdf
Is very good explained, tell me about problems.
Moidom,
I followed the steps in AN3765.pdf up till Section 2.3. Do I have to follow the other sections?
I already replied to your reply on my other thread
https://community.freescale.com/thread/64183
If you have time please I would really appreciate your help. Thank you.
bbjh1
From pages 34 to 42