Hello,
I use USB-ML-CFE Rev.C from PE Micro for programming my aplication with CodeWarrior 7.1 on a MCF52230 coldfire.
It's works fine month ago.
But since I've updated with new 7.2 version, on the status window, when I tried to erase flash memory, there is: "Error: initialization failed."
Someone have an idea to help me ?
I don't know what to do !!!
Thank you for help,
Thomas.
I'm getting the same failure with Code Warrior 7.2 using USB-ML-CFE rev. C. Trying to connect to a M52235EVB board.
I can make the project in CW and then flash it to the target with P&E's PROGCFZ starter addition and everyhing runs fine on the board, but I can't get it to connect/flash directly from CW.
Any input on things to try would be welcome.
Hi,
I have the same problem, but my firmware is the revicion "D".
Is any sugestion out there?
Thank you Ariel