Hi,
Has anyone successfully used PE beans with Xgate? Apparenty PE (2.98) does not have support for Xgate yet. I've used PE to generate SCI (uart) code for hadling interrupts/events. I need the interrupt (and all events/ functions assoicated with it) to be redirected to xgate.
The normal way (without using beans) would be:
1. Direct the interrupt event to the XGATE. (RQST bit)
2. Create a thread to handle the interrupt.(i.e. an interrupt handler)
3. Initialize the XGATE interrupt vector table to point to the thread.
What do i need to modify in the PE genereated code to achieve the same?
Thanks.
Ravi
Solved! Go to Solution.