Hi,
I am using
mpc8548e custom made board with nor flash s29al016d90tfi01, using usb tap , the cfg file used is '8548CDS_sram_flash.cfg', attached the installed plugin for the code warrier and related installs.
i was using initally 1.2GHz ceramic bga for the design and the jtag was fine i could flash the nor and now i used 1.3GHz plastic bga and this is the error message i get when i try to connect the jtag - attached the log file for the error message.
i am using the -> "tool -> flash programmer " to program the flash.
i am not able to pin point as to what is the issue and is the identified core is correct -> darco/m hip8????.
Can some one give me pointers for me to go ahead.
thanks
Prasad
Hi Prasad,
Whether dropping in a new chip into an old socket or bringing up a new board, it's a good idea to verify the low-level JTAG interface is functioning properly. You should have a file called 'idcode.tcl' in your \ccs\bin folder. Double-click on ccs.exe in that folder to launch CCS manually, then double-click on the CCS Console icon when it appears in your Windows Tooltray to bring up the CCS Console. In the Console enter 'source idcode.tcl' to load in a diagnostic routine, select your USB TAP, then enter 'scanboard' to run the diagnostic and post your results. We need to see a valid JTAG ID code from this test before we can proceed.
Regards,
Ron