Hi,
I want to change from gdb on Linux PC to CW on Windows PC platform.
-my C applications run under real time RTEMS OS on PPC processors (MPC8xx now,
MPC8XXX in the future).
-I have to use the gnu gcc compiler since RTEMS comes with the appropriate gnu tools versions.
-I'm using in-house built boards.
-I use the BDM debug port (OCD).
Is BASIC suite OK or do I need the STANDARD?
Thanks in advance!
Go to the product web page for the Power Architecture suite and download the Quick Reference Guide for CodeWarrior Suites, which is a PDF (Acrobat) file. You can check to see which suite best meets the requirements for your project.
---Tom