AnsweredAssumed Answered

MCF52233

Question asked by Lakshmi Singh on Feb 15, 2010
Latest reply on Feb 15, 2010 by Lakshmi Singh

Hi,

 

We have developed two products using Freescale MPU, MCF52233 & MCF52212. (Using EMBEDDED C)

 

Now we are designing another product to be developed, using MCF52233 & MCF52211 64 pin package. For this, we would like to switch from Embedded C to Embedded C++.

 

Is EMBEDDED C++ recommended to use for these two processors? Our MAIN goal is to use MULTI THREADING  RTOS, to achieve multi tasking using these two processors.

 

Please Note:

 

MCF52211: Flash/SRAM = 128/16k Bytes

MCF52233: Flash/SRAM = 256/32k Bytes

 

Is it possible to port MULTITHREADING RTOS (like, interniche coldfire_lite) for 52211 processor & achieve multi tasking? Has anyone tried this out?

 

Has anyone tried to use EMBEDDED C++ for either of the two processors (52211/52233)?

 

Thanks,

Lakshmi

Outcomes