USB-Bluetooth Adapter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB-Bluetooth Adapter

Jump to solution
1,501 Views
Babak
Contributor I

Hi all,

 

i have the 52259 demo board, with codewarrior 7.1 and Freescale MQX 3.0. my task is to connect Wiimote to the board and i imagine one the solutions for this is the USB-Bluetooth adapter (the other might be using the Ethernet interface of the board but i'm still not sure how close Ethernet and bluetooth are and how difficult it is to do)

 

so for start i need some driver for connecting a USB-Bluetooth adapter to the board..as i've understood there is no support for this in the existing libraries though there might be support for low-level functions...

 

so any suggestions? anywhere i can find the driver i need? or should i go through writing the driver myself?!

Labels (1)
Tags (1)
0 Kudos
1 Solution
308 Views
JuroV
NXP Employee
NXP Employee

Hi Babak. Unfortunatelly, no such driver is written in MQX yet.

Message Edited by JuroV on 2010-02-08 09:45 AM

View solution in original post

0 Kudos
1 Reply
309 Views
JuroV
NXP Employee
NXP Employee

Hi Babak. Unfortunatelly, no such driver is written in MQX yet.

Message Edited by JuroV on 2010-02-08 09:45 AM
0 Kudos