Hi,
I'm trying to rebuild the Freescale MQX 3.4\config\twrmcf51cn\build_libs.mcp
As the project is generating some errors, I tried to build saparately.
Freescale MQX 3.4\mqx\build\codewarrior\PSP_twrmcf51cn.mcp
In the Target options, I've selected build all as it complains about the target. But the errors remain.
#ifdef __STDABI__
#if __STDABI__ == 0
#error Project for standard ABI, but compiler do not use standard ABI
It seems to be a simple error related to compiler options. Anyone could help?
Solved! Go to Solution.
A Few hours later...
Unistalled Mqx 3.4, updated codewarrior suites, installed 6.2.2 patch that shows at FSL updater as a web-ste.
Then reinstalled and worked perfectly.
I think that I opened the project at CW 7.1 and the project was updated and doesn´t worked at 6.3,6.2.
Solved!
A Few hours later...
Unistalled Mqx 3.4, updated codewarrior suites, installed 6.2.2 patch that shows at FSL updater as a web-ste.
Then reinstalled and worked perfectly.
I think that I opened the project at CW 7.1 and the project was updated and doesn´t worked at 6.3,6.2.
Solved!