I am currently using codewarrior V2.5 for PowerPC with the MPC5607B which has a Z0 core with no hardware floating point support.
I am using the software floating point option and I am able to calculate correctly floating point math operations with no problem. The issue is when I send the calculated result back to the calling function the variable in the calling function that is expected to be equated to the return result is not getting set to the value calculated. I have included the following libraries in my project:
MSL_C.PPCEABI.bar.VS.UC.a
Runtime.PPCEABI.VS.UC.a
It is like the GPR register assignment is not looking at the right register for the return parameter.
I have converted the function to return UINT32 and it does return the parameter appropriately but I need to be able to return floating point numbers. Thank you!
Solved! Go to Solution.
Thanks for the reply. I did try what you suggested and it did work. Then I looked carefully at at the header files that I am including in my main and noticed that I had forgotten to add the header file that defines the function that I am using to the main.c. I am guessing that the compiler was redifining the function call since it did not have the appropriate header file included. Once I did that my float return did work so thank you for help and time. It did help point me in the right direction.
But this raises another question. Why did the compiler not warn me of the redefinition. I have used codewarrior before and it has in the past warn me of redefinitions. I tried excluding another file and it did not warn me of that either. Is there a setting that I need to enable to turn on warnings?
Thanks again!
Hello
Are you sure the library files you are using matches your project settings?
Please refer to "{Install}\Help\PDF\Power Architecture Build Tools Reference.pdf" chapter "Libraries and Support Code", section "Main Standard Libraries" -> "Choosing an MSL library" for information on encoding used for library names.
Make sure the library you are selecting matches your actual compilation option...
CrasyCat
I have looked at this and the libraries that I am using are the default ones that came in when I set up the project based on the option that I chose. Also, it has been my experience that if I choose a library that does not conform to the project settings I get warnings from the compiler.
Either way, I have tried different libraries based on the table that you referenced in your reply with no success. I have been able to pass the result by passing the address of the float variable thru the parameter list which is a possible work around but I would need to change a number of function calls that use the return at the end of the function to pass a result back.
Any other ideas? Thank you for you help!
johna123
Hi Johana123,
I've tested this using software floating point sum (MPC5604P):
1) created new project using ProjectWizard, enable software floating point.Default libs (Runtime.PPCEABI.VS.UC.a, MSL_C.PPCEABI.bare.VS.UC.a)
2) add fsum() into main.c:
volatile float x,y,f;
float fsum(float a, float b)
{
return a+b;
}
int main(void) {
volatile int i = 0;
x = 3.14;
y = 2.5;
f = fsum(x,y);
}
3) compile and check in the P&E debugger.
It works as expected.
Could you possibly try the same example on your side.
If it works then please post your code here to review.
Stanish
Thanks for the reply. I did try what you suggested and it did work. Then I looked carefully at at the header files that I am including in my main and noticed that I had forgotten to add the header file that defines the function that I am using to the main.c. I am guessing that the compiler was redifining the function call since it did not have the appropriate header file included. Once I did that my float return did work so thank you for help and time. It did help point me in the right direction.
But this raises another question. Why did the compiler not warn me of the redefinition. I have used codewarrior before and it has in the past warn me of redefinitions. I tried excluding another file and it did not warn me of that either. Is there a setting that I need to enable to turn on warnings?
Thanks again!