Hi, We have used MCF52233 processor for Master board & MCF52212 for Slave.
We have completed the implementation & testing of the project & now in RELEASE cycle. In the Customer's site Field Application Engineer will not be provided with the code warrior IDE to download the firmware using BDM.
We need to create a setup file, which can used to program incremental versions of firmware to the PCBs.
Could you please tell us, what are the supporting files required to create the build?
FYI: MCF52233 uses Interniche TCPIP_ClodeFire_Lite multithreading RTOS project as a code base. MCF52212 is not multithreading RTOS
Hi
A SREC loader (requires about 10k space) for these devices is available at www.uTasker.com. User's guide http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.PDF
It also supports loading via USB and Ethernet (optionally encrpted) but not as stand-alone loader (requires 2k in this case).
Regards
Mark
Hi ,
u can also use CFlasher for loading program thru BDM.
u can also create separate exe file which read ur s19/Bin file and increment ur FIRMWARE VERSION or may be PCB nos. n then load it
Hi,
Thank you for the quick response.
Could you plaese tell me, where can I get CFlasher from?