LTIB is showing error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LTIB is showing error

2,225 Views
admin
Specialist II
Hello, I am trying to install gstreamer codec in IMX51 board. for that i downloaded onr document from website. I folloed the steps accourding to that document. In that when i tried to install LTIB by giving command ./ltib. It is not working. All other things are fine. I copies all the things in /opt and i replaced the spec files. Now my error is [code]ariem@ariem-desktop:~/Desktop/plugins/L2.6.28_4.5.1_SDK_Aug2009_source/ltib$ ./ltib sh: tclsh: command not found ltib cannot be run because one or more of the host packages needed to run it are either missing or out of date or not in ltib's standard path. Please install/upgrade these packages on your host. If you have your own utilities in non-standard paths, please add an entry into the .ltibrc file for example: %path_std /usr/local/bin:/usr/bin:/bin:/usr/bin/X11:/usr/X11R6/bin:/my/own/exes Package Minimum ver Installed info ------- ----------- --------------- zlib-devel 0 not installed rpm 0 not installed rpm-build 0 not installed m4 0 not installed bison 0 not installed tcl 0 not installed Died at ./ltib line 1397. traceback: main::host_checks:1397 main:542 Started: Tue Dec 22 18:54:26 2009 Ended: Tue Dec 22 18:54:27 2009 Elapsed: 1 seconds Build Failed Exiting on error or interrupt ariem@ariem-desktop:~/Desktop/plugins/L2.6.28_4.5.1_SDK_Aug2009_source/ltib$ [/code]
Tags (1)
0 Kudos
1 Reply

826 Views
Apple92
Contributor II

Hello,

 

The first launch of ./ltib is always the most difficult of all steps required to get a working toolchain.

 

According to what I read:

 

"zlib-devel 0 not installed rpm 0 not installed rpm-build 0 not installed m4 0 not installed bison 0 not installed tcl 0 not installed Died at ./ltib line 1397. traceback: main::host_checks:1397 "

 

You should "apt-get install" those packages.

 

Which linux host flavour are you using? (Debian, Ubuntu, Fedora, etc).

 

You should subscribe to ltib.org mailing list: http://ltib.org/resources-mailing-list and submit your LTIB-related questions on this mailing list.

 

Regards,

Franz

0 Kudos