Dear pgo,
I have heard in the recent FTF that Freescale is migrating Codewarrior to eclipse paltform, so what amount of changes will be there at the drivers at the PC side and as well as the firmware side, if USBDM have to work on the eclipse paltform.
Thanks and Regards
Raghavendra
Dear raghu123,
No idea!
If Freescale continue to support the TBDML/OSBDM interface and provide the source for the interface DLLs (TBDML.dll & opensourceBDM.dll or equivalent) for the eclipse version then USBDM will continue to operate or be adaptable to that interface.
I have also written a compatibility interface for the newer OSBDM-JM60 so the above would also apply for this one if the sources are available.
Beyond that I can't say anything since I don't have any knowledge of the intended Eclipse interface.
You had better ask Freescale what their intentions are.
bye
Dear pgo,
Thanks for the information , i hope Freescale continues with USBDM for eclipse platform.
bye
Hello all,
I have build a few Open source BDM based on JB16 and i would like to ask if does someone knows if there is a dll for codewarrior 10 based on eclipse,.
Thanks in advance.