Hi,
I tried to using std::string in my application ( MQX 3.4.0)
However whenever I include:
#include <string>
I got a lot of compiling error. Could anyone tell me how to solve this problem?
Thanks
J.
Hello,
this is C++ standard. It is not applicable for MQX.
If you want to use some C style string functions, try this:
#include <string.h>
Regards,
PetrM
PetrM,
I did use C++ in my code.
I believe MQX can be compiled working with C++ application. ( the Former project I did used C++ ( CodeWarrior 6.3+ ColdFire5329+MQX2.50)).
Regards,
Jeff
In MQX, it redefines getwc, io_fgets, FILE etc, when I include <string> to use std::string , that causes compiling error......
other C++ features so far no problem.
Anyone sees similiar problem? I wish in next MQX release, it can provide examples for using C++ with MQX.
Typically we provide technical support for companies who have a support contract, however we do try to help users out in advance of a support contract if they are just starting out or evaluating our services. Please send a note to info@embedded-access.com with your contact information, and then we can take a look at it.
Doug
Embedded Access Inc.