Hi All,
I'm using CW-6.4 Build 6.
My controller is MCF5485.
Recently I was successful with making a small LED blink program work standalone on my target board.
(Bootloading was OK!!) ...
Now I have a problem when I have to burn my custom code.
I'm able to burn the S-rec file into Flash using the Flash programmer.
I also verified with the "Hardware DIag" , that the address 0xFE000000(The location of my code!)
has the S-record file....
But when I try to download the code, After downloading I get the error->
"COULD NOT SET PC TO ENTRY POINT"
I suspect my linker file, as other things seem to be OK.....
Please help me out with my linker file....
LCF FILE::
#/********************************************************************/ #/**************************FPRO3000-Linker***************************/ #/********************************************************************/ #/********************************************************************/ #/**************************MEMORY sections***************************/ #/********************************************************************/ MEMORY { sdram (RWX) : ORIGIN = 0x00000500, LENGTH = 0x02000000 mbar (RWX) : ORIGIN = 0x10000000, LENGTH = 0x00040000 boot_flash (RWX) : ORIGIN = 0xFE000000, LENGTH = 0x02000000 } SECTIONS { #/********************************************************************/ #/****************************Definitions*****************************/ #/********************************************************************/ .bootCode : { vectors.s (.text) *(.text) *(.rodata) .= ALIGN(0x8); } > boot_flash __end_of_text = .; ___DATA_ROM = __end_of_text; ___CODE_ROM = __end_of_text; ___CODE_RAM = ADDR(sdram); ___DATA_RAM = ADDR(sdram); .sdram : AT(ADDR(.bootCode) + SIZEOF(.bootCode)) { *(.exception) .= ALIGN(0x8); __exception_table_start__ = .; EXCEPTION __exception_table_end__ = .; ___sinit__ = .; STATICINIT __START_DATA = .; *(.data) __START_SDATA = .; *(.sdata) __END_DATA = .; ___DATA_END = .; __END_SDATA = .; . = ALIGN(0x8); __SDA_BASE = .; } > sdram .bss: { ___BSS_START = .; __START_SBSS = .; *(.sbss) *(SCOMMON) __END_SBSS = .; __START_BSS = .; *(.bss) *(COMMON) __END_BSS = .; ___BSS_END = .; ___HEAP_START = .; ___heap_addr = ___HEAP_START; ___heap_size = 0x02000000; ___HEAP_END = ___HEAP_START + ___heap_size; ___SP_END = ___HEAP_END; ___SP_INIT = ___SP_END + (10*1024); __SP_INIT = ___SP_INIT; . = ALIGN(0x8); } >>sdram ___MBAR = ADDR(.mbar); __MBAR = ___MBAR; ___SDRAM = ADDR(.sdram); ___SDRAM_SIZE = 0x08000000; ___BOOT_FLASH = ADDR(.bootCode); ___BOOT_FLASH_SIZE = 0x00200000; ___FLASH = ___BOOT_FLASH; _romp_at = ___DATA_ROM + SIZEOF(.sdram); .romp : AT(_romp_at) { __S_romp = _romp_at; WRITEW(___CODE_ROM); # FLASH CODE Address WRITEW(___CODE_RAM); # SDRAM CODE Address WRITEW(SIZEOF(.bootCode));# CODE Size WRITEW(___DATA_ROM); # FLASH Initialized DATA Address WRITEW(___DATA_RAM); # SDRAM Initialized DATA Address WRITEW(SIZEOF(.sdram)); # DATA Size WRITEW(0); # NULL Last Entry WRITEW(0); # NULL Last Entry WRITEW(0); # NULL Last Entry } ___free_mem = ___heap_addr + ___heap_size; # for threadx }
Please post your comments on the file....
Solved! Go to Solution.
Hello,
In your LCF file, the S_romp structure initialization looks strange, the source and destination address are the same for both CODE and DATA:
___DATA_ROM = ___CODE_ROM = __end_of_text;
___DATA_RAM = ___CODE_RAM = ADDR(sdram);
S_romp is used by the ROMtoRAM copy routine at startup
Check if your code uses the ROMtoRAM copy routine at startup.
I Hope this helps..
Bye
<< Freescale MCF5234/35 with CodeWarrior 6.4>>
Hello,
In your LCF file, the S_romp structure initialization looks strange, the source and destination address are the same for both CODE and DATA:
___DATA_ROM = ___CODE_ROM = __end_of_text;
___DATA_RAM = ___CODE_RAM = ADDR(sdram);
S_romp is used by the ROMtoRAM copy routine at startup
Check if your code uses the ROMtoRAM copy routine at startup.
I Hope this helps..
Bye
<< Freescale MCF5234/35 with CodeWarrior 6.4>>
Hello
Did you define some breakpoints or watchppoints in your application? How many?
Here your application is loaded into ROM. So the debugger cannot use software breakpoint. It needs to use hardware breakpoints.
According to the message I assume there are not enough hardware breakpoints available on board to set a BP on main function (as specified in the "Debugger Settings" panel).
CrasyCat