AnsweredAssumed Answered

Can't program M52259 demo board

Question asked by Mark Armbrust on Oct 20, 2009
Latest reply on Sep 26, 2011 by Jesus Lopez

Hello,

I'm using CW 7.1 build 14 with patch 7.1.2 build 11.

I've done the JM60 FW update per the 7.1.2 readme.

I've downloaded and installed MQX 3.3.

I can run the pre-programmed web_hvac demo.

I make a small change to the demo (change CD command to CDX) build and run.  Same old demo is running.  OK, I'm new to CW; obviously it doesn't automatically program the target -- it'd be nice if it told me the target was out of date, but whatever.

 

The flash programmer is initially configure for some incorrect target so I change it to use

52259 / Coldfire v2-v4 JM60 OSBDM

C:\Program Files\Freescale\CodeWarrior for ColdFire V7.1\ColdFire_Support\Initialization_Files\M52259DEMO.cfg

and set the flash config to CFM_MCF5225X_512

 

All attempts to blank-check / erase / program result in the error message

"ColdFire GDI Protocol Adapter : An error occurred while trying to write memory"

 

What am I doing wrong?

Outcomes