Hi everyone,
I am using a CodeWarrior Development Studio for DSC56800/E version 8.1.1a. (56F8037, 56F8025 etc dscs).
I want to be able to compile and create an elf and .S file without using IDE. I was able to create a makefile
using Project - Export Project as GNU Makefile. The question is how do I use this file to compile and create .elf and .S?
Thanks,
Ansi_Cartman
Look in the following directories:
{CodeWarrior Installation}\DSP56800x_EABI_Tools\command_line_tools\ and study the contents of mwld56800e.txt. This has information on using the command line linker and its control switches. The -srec switch should generate a S-record file for you.
In the {CodeWarrior Installation}\Help directory, look for the Build Tools Reference manual (56800x_Build_Tools_Reference.pdf) and check out the chapter, Using the Build Tools on the Command Line for more information.
---Tom
Hi Tom,
Can you give a simple example siting how this can be done. I have attached a sample code. Can you show how I can compile this and generate the -srec.
Thanks in advance,
Ansi_Cartman
Hi,
Attached you will find an example.
Have a look to the .bat file.
Hope this will help you.
Regards
Pascal