Solved! Go to Solution.
So, I have solved this (a bit of a kludge). I temporarily made the non-administrative user an admin. Then installed for him, and changed him back to a member of PowerUsers group. Seems to work for now.
--- RAM
So, I have solved this (a bit of a kludge). I temporarily made the non-administrative user an admin. Then installed for him, and changed him back to a member of PowerUsers group. Seems to work for now.
--- RAM
Hello,
it seems this was in issue in the InstallShield (the installation program) used in CW 5.9. To my understanding this has been resolved in CW 6.1 as this uses the new InstallShield which has resolved this.
BK
Perhaps I've overlooked something, but the only edition I see for HCS12 family is 5.9; the version 6.1 is for other chips, not the HCS12 family. Someone please correct me if I'm wrong on this. Also, is there a patch to fix this problem in 5.9 if it is a known issue?
-- RAM
Version 5.9 is the IDE version, not the actual version of the tools. To get the tools version number, select Help > About Freescale CodeWarrior > Installed Products. If you downloaded the Special Edition of the HC12 tools recently, it has to be version 5. You might file a service request to have this installer feature fixed or added.
Also, when posting a question, remember to include the hardware target name (such as HC(S)08 or HCS12(C)) along with the version number.
---Tom
Hi RAM,
I (wrongly) assumed you are using CW for MCU/HCS08. My reply was targeting to that product line, and not the S12 one.
BK