Hi,
I am generating a kernel by using LTIB configured for iMx35 3-Stack board.
There happens a weird error. When building udev, LTIB tries to patch a file.
nevertheless, the patch file md5 mismatches the MD5 value in the patch.md5 file.
Thus, LTIB renames the file with the bad extension and stops. I launch again
./ltib and LTIB tries to connect to the GPP on bitshrine server. The issue is that
this file does not exist on the current GPP. This file is udev-117-imx-lowcase2.patch
whereas udev-117-imx-lowcase.patch (yes, the same without the "2") exists !
Did someone face the same issue?
here is the script extracted from the error output.
Processing: udev
==================
Build path taken because: no prebuilt rpm,
ERROR: md5sum mismatch, re-naming /opt/freescale/pkgs/udev-117-imx-lowcase2.patch to /opt/freescale/pkgs/udev-117-imx-lowcase2.patch.bad, please re-try
Can't get: udev-117-imx-lowcase2.patch at ./ltib line 786.
f_buildrpms() returned an error, exiting
traceback:
main:557
Started: Wed Sep 16 18:16:16 2009
Ended: Wed Sep 16 18:16:17 2009
Elapsed: 1 seconds
These packages failed to build:
udev
Build Failed
Exiting on error or interrupt
Second launch:
Processing: udev
==================
Build path taken because: no prebuilt rpm,
Testing network connectivity
OK GPP:
Try udev-117-imx-lowcase2.patch from the GPP
http://bitshrine.org/gpp/udev-117-imx-lowcase2.patch:
18:17:33 ERROR 404: Not Found.
Can't get: udev-117-imx-lowcase2.patch at ./ltib line 786.
f_buildrpms() returned an error, exiting
traceback:
main:557
Started: Wed Sep 16 18:17:30 2009
Ended: Wed Sep 16 18:17:33 2009
Elapsed: 3 seconds
These packages failed to build:
udev
Build Failed
Exiting on error or interrupt
Regards,
Apple92
Solved! Go to Solution.
Finally, there are still bad MD5 files in the package shipment. I computed them with md5sum commands and now the build chain is OK.
Thus, if you use Freescale iMX35 CD, check the MD5 files and compute them yourself if you want to have clean source files.
Regards
Finally, there are still bad MD5 files in the package shipment. I computed them with md5sum commands and now the build chain is OK.
Thus, if you use Freescale iMX35 CD, check the MD5 files and compute them yourself if you want to have clean source files.
Regards