AnsweredAssumed Answered

Updating MC1322x boards

Question asked by Mohamed Hedi Daouas on Jul 22, 2009
Latest reply on Sep 15, 2009 by Michael Conover

Hi everyone, 

 

I'm new to this forum and I hope to find help here. I have a very big problem. I have two freescale MC1322x boards (network and sensor node boards) and everytime I reprogram them with IAR EWARM 5.4 by clicking clean after rebuild all after make and finally debug, the application works but after I swith off/on it is replaced by the pre-installed application (weather station). Do I need everytime to use the firmware loader of the Test Tool to replace the pre-installed app ?

 

Another problem is that sometimes I have network problems even if I never touch the source codes given with codebases. For example with MyStarNetwork application, the network node that is connected with usb is detected by the application but after I link the sensor node it stays for some seconds then is inactive and goes away. Same problems were faced before with Weather Station Application but no more now. Very strange !

Outcomes