renee straney

MCF52233CAF60 and monitoring my power supplies

Discussion created by renee straney on Jul 22, 2009
Latest reply on Jul 22, 2009 by Guest

Hello,

I have two +5 volt power supplies in my product.  One is used as a redundant supply so only one is active at a time.  I want to report to the user via my command line the status of the power supplies.   

 

I really only need to report if they are "up" - not necessarily their exact voltages.  

 

Can anyone share how this is generally done? 

 

Here are my first ideas:

 

Use 2 voltage supervisors to monitor each supply and run their outputs to my 52233 and just read the pins for the correct logic level. 

 

I also thought of running the voltages from the supplies over to the processors A/D inputs (Via a voltage divider since it appears the 52233 can read up to Vrefh which cannot exceed VDDA.) and sampling them.

 

Or are there other ways to accomplish this? 

 

Thanks

Renee

Outcomes