How to generate .a2l file from codewarrior .map file?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to generate .a2l file from codewarrior .map file?

Jump to solution
7,441 Views
hbch
Contributor III
I am using codewarrior for MPC55xx V2.4 and the target is MPC5633m. The .map file generated by the linker can not be converted to .a2l file by Vector ASAP2 Editor which is a tool of CANape. Can anyone help me?
Labels (1)
0 Kudos
1 Solution
3,014 Views
hbch
Contributor III
I am sory to report that the solution does not work at all. The A2l misses variables' names and their addresses. If in standard format, the a2l file can get the variables' names but no addresses. Please refer to the attached file.
Message Edited by hbch on 2009-07-23 12:50 PM

View solution in original post

0 Kudos
3 Replies
2,179 Views
puliufeng
Contributor I

I met the same problem,how to slove it?  Need help

0 Kudos
3,014 Views
ronco
NXP Employee
NXP Employee

We haven't used the Vector ASAP2 Editor before but we just installed a demo and the only suggestion we have is to set the  MAP file definition  to Metrowerks.  Take a look at the attached screenshot for an example.  I hope this helps.

 

-Ron

0 Kudos
3,015 Views
hbch
Contributor III
I am sory to report that the solution does not work at all. The A2l misses variables' names and their addresses. If in standard format, the a2l file can get the variables' names but no addresses. Please refer to the attached file.
Message Edited by hbch on 2009-07-23 12:50 PM
0 Kudos